Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static NormalToToolAxisMoveBuilder.Orientation |
NormalToToolAxisMoveBuilder.Orientation.ALONG_VECTOR
Along Vector
|
static NormalToToolAxisMoveBuilder.Orientation |
NormalToToolAxisMoveBuilder.Orientation.TOWARDS_POINT
Towards Point
|
Modifier and Type | Method and Description |
---|---|
NormalToToolAxisMoveBuilder.Orientation |
NormalToToolAxisMoveBuilder.moveType()
Returns the normal type
License requirements: None. |
static NormalToToolAxisMoveBuilder.Orientation |
NormalToToolAxisMoveBuilder.Orientation.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NormalToToolAxisMoveBuilder.Orientation |
NormalToToolAxisMoveBuilder.Orientation.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NormalToToolAxisMoveBuilder.Orientation[] |
NormalToToolAxisMoveBuilder.Orientation.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NormalToToolAxisMoveBuilder.setMoveType(NormalToToolAxisMoveBuilder.Orientation normaltype)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.