Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static NcmWedmBuilder.LeadOutSameAsLeadInTypes |
NcmWedmBuilder.LeadOutSameAsLeadInTypes.NO
not the same
|
static NcmWedmBuilder.LeadOutSameAsLeadInTypes |
NcmWedmBuilder.LeadOutSameAsLeadInTypes.YES
the same as lead in
|
Modifier and Type | Method and Description |
---|---|
NcmWedmBuilder.LeadOutSameAsLeadInTypes |
NcmWedmBuilder.leadOutSameAsLeadIn()
Returns the lead out same as lead in
License requirements: cam_base ("CAM BASE") . |
static NcmWedmBuilder.LeadOutSameAsLeadInTypes |
NcmWedmBuilder.LeadOutSameAsLeadInTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NcmWedmBuilder.LeadOutSameAsLeadInTypes |
NcmWedmBuilder.LeadOutSameAsLeadInTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NcmWedmBuilder.LeadOutSameAsLeadInTypes[] |
NcmWedmBuilder.LeadOutSameAsLeadInTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NcmWedmBuilder.setLeadOutSameAsLeadIn(NcmWedmBuilder.LeadOutSameAsLeadInTypes sameAsLeadIn)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.