Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static NcmWedmBuilder.LeadOutMethodTypes |
NcmWedmBuilder.LeadOutMethodTypes.ANGULAR
angular lead out
|
static NcmWedmBuilder.LeadOutMethodTypes |
NcmWedmBuilder.LeadOutMethodTypes.CIRCULAR
circular lead out
|
static NcmWedmBuilder.LeadOutMethodTypes |
NcmWedmBuilder.LeadOutMethodTypes.DIRECT
direct lead out
|
static NcmWedmBuilder.LeadOutMethodTypes |
NcmWedmBuilder.LeadOutMethodTypes.SAME_AS_LEAD_IN
same as lead in
|
Modifier and Type | Method and Description |
---|---|
NcmWedmBuilder.LeadOutMethodTypes |
NcmWedmBuilder.leadOutMethod()
Returns the lead_out_method
License requirements: cam_base ("CAM BASE") . |
static NcmWedmBuilder.LeadOutMethodTypes |
NcmWedmBuilder.LeadOutMethodTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NcmWedmBuilder.LeadOutMethodTypes |
NcmWedmBuilder.LeadOutMethodTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NcmWedmBuilder.LeadOutMethodTypes[] |
NcmWedmBuilder.LeadOutMethodTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NcmWedmBuilder.setLeadOutMethod(NcmWedmBuilder.LeadOutMethodTypes leadOutMethod)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.