Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static NcmWedmBuilder.LeadInMethodTypes |
NcmWedmBuilder.LeadInMethodTypes.ANGULAR
angular lead in
|
static NcmWedmBuilder.LeadInMethodTypes |
NcmWedmBuilder.LeadInMethodTypes.CIRCULAR
circular lead in
|
static NcmWedmBuilder.LeadInMethodTypes |
NcmWedmBuilder.LeadInMethodTypes.DIRECT
direct lead in
|
Modifier and Type | Method and Description |
---|---|
NcmWedmBuilder.LeadInMethodTypes |
NcmWedmBuilder.leadInMethod()
Returns the lead_in_method
License requirements: cam_base ("CAM BASE") . |
static NcmWedmBuilder.LeadInMethodTypes |
NcmWedmBuilder.LeadInMethodTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NcmWedmBuilder.LeadInMethodTypes |
NcmWedmBuilder.LeadInMethodTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NcmWedmBuilder.LeadInMethodTypes[] |
NcmWedmBuilder.LeadInMethodTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NcmWedmBuilder.setLeadInMethod(NcmWedmBuilder.LeadInMethodTypes leadInMethod)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.