Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static NcmTurnThreadBuilder.LocalReturnModes |
NcmTurnThreadBuilder.LocalReturnModes.NONE
None
|
static NcmTurnThreadBuilder.LocalReturnModes |
NcmTurnThreadBuilder.LocalReturnModes.NUMBER_OF_PASSES
Number of Passes
|
static NcmTurnThreadBuilder.LocalReturnModes |
NcmTurnThreadBuilder.LocalReturnModes.NUMBER_OF_STARTS
Number of Starts
|
Modifier and Type | Method and Description |
---|---|
NcmTurnThreadBuilder.LocalReturnModes |
NcmTurnThreadBuilder.localReturnFinishMode()
Returns the Local Return Finish Mode
License requirements: None. |
NcmTurnThreadBuilder.LocalReturnModes |
NcmTurnThreadBuilder.localReturnRoughMode()
Returns the Local Return Rough Mode
License requirements: None. |
static NcmTurnThreadBuilder.LocalReturnModes |
NcmTurnThreadBuilder.LocalReturnModes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NcmTurnThreadBuilder.LocalReturnModes |
NcmTurnThreadBuilder.LocalReturnModes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NcmTurnThreadBuilder.LocalReturnModes[] |
NcmTurnThreadBuilder.LocalReturnModes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NcmTurnThreadBuilder.setLocalReturnFinishMode(NcmTurnThreadBuilder.LocalReturnModes localReturnFinishMode)
License requirements: cam_base ("CAM BASE") . |
void |
NcmTurnThreadBuilder.setLocalReturnRoughMode(NcmTurnThreadBuilder.LocalReturnModes localReturnRoughMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.