Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static NcmTransferBuilder.TraverseTypes |
NcmTransferBuilder.TraverseTypes.DIRECT
traverse direct
|
static NcmTransferBuilder.TraverseTypes |
NcmTransferBuilder.TraverseTypes.LOWEST_SAFE_Z
traverse at lowest safe z
|
static NcmTransferBuilder.TraverseTypes |
NcmTransferBuilder.TraverseTypes.SAME
traverse setting from between regions
|
static NcmTransferBuilder.TraverseTypes |
NcmTransferBuilder.TraverseTypes.SHORTEST_TO_CLEARANCE
traverse shortest to clearance
|
static NcmTransferBuilder.TraverseTypes |
NcmTransferBuilder.TraverseTypes.SMOOTH
traverse smooth spline
|
Modifier and Type | Method and Description |
---|---|
NcmTransferBuilder.TraverseTypes |
NcmTransferBuilder.traverseType()
Returns the traverse types
License requirements: None. |
static NcmTransferBuilder.TraverseTypes |
NcmTransferBuilder.TraverseTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NcmTransferBuilder.TraverseTypes |
NcmTransferBuilder.TraverseTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NcmTransferBuilder.TraverseTypes[] |
NcmTransferBuilder.TraverseTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NcmTransferBuilder.setTraverseType(NcmTransferBuilder.TraverseTypes newValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.