Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static NcmScEngRetBuilder.MeasureFromTypes |
NcmScEngRetBuilder.MeasureFromTypes.DISTANCE
Measure from distance
|
static NcmScEngRetBuilder.MeasureFromTypes |
NcmScEngRetBuilder.MeasureFromTypes.PLANE
Measure from user-defined plane
|
Modifier and Type | Method and Description |
---|---|
NcmScEngRetBuilder.MeasureFromTypes |
NcmScEngRetBuilder.measureFrom()
Returns the height or length from which engage linear/helical/plunge is measured
License requirements: None. |
static NcmScEngRetBuilder.MeasureFromTypes |
NcmScEngRetBuilder.MeasureFromTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NcmScEngRetBuilder.MeasureFromTypes |
NcmScEngRetBuilder.MeasureFromTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NcmScEngRetBuilder.MeasureFromTypes[] |
NcmScEngRetBuilder.MeasureFromTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NcmScEngRetBuilder.setMeasureFrom(NcmScEngRetBuilder.MeasureFromTypes newValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.