Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static NcmPlanarEngRetBuilder.IfEngageDoesNotFitTypes |
NcmPlanarEngRetBuilder.IfEngageDoesNotFitTypes.PLUNGE
Plunge
|
static NcmPlanarEngRetBuilder.IfEngageDoesNotFitTypes |
NcmPlanarEngRetBuilder.IfEngageDoesNotFitTypes.SKIP
Skip
|
Modifier and Type | Method and Description |
---|---|
NcmPlanarEngRetBuilder.IfEngageDoesNotFitTypes |
NcmPlanarEngRetBuilder.ifEngageDoesNotFit()
Returns the type to handle area if engage does not fit
License requirements: None. |
static NcmPlanarEngRetBuilder.IfEngageDoesNotFitTypes |
NcmPlanarEngRetBuilder.IfEngageDoesNotFitTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NcmPlanarEngRetBuilder.IfEngageDoesNotFitTypes |
NcmPlanarEngRetBuilder.IfEngageDoesNotFitTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NcmPlanarEngRetBuilder.IfEngageDoesNotFitTypes[] |
NcmPlanarEngRetBuilder.IfEngageDoesNotFitTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NcmPlanarEngRetBuilder.setIfEngageDoesNotFit(NcmPlanarEngRetBuilder.IfEngageDoesNotFitTypes newValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.