Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static NcmPlanarBuilder.TransferBetweenLevelsTypes |
NcmPlanarBuilder.TransferBetweenLevelsTypes.CLEARANCE
clearance
|
static NcmPlanarBuilder.TransferBetweenLevelsTypes |
NcmPlanarBuilder.TransferBetweenLevelsTypes.DIRECT
direct
|
static NcmPlanarBuilder.TransferBetweenLevelsTypes |
NcmPlanarBuilder.TransferBetweenLevelsTypes.PREV_PLANE
previous plane
|
Modifier and Type | Method and Description |
---|---|
NcmPlanarBuilder.TransferBetweenLevelsTypes |
NcmPlanarBuilder.transferBetweenLevelsType()
Returns the transfer between levels type
License requirements: None. |
static NcmPlanarBuilder.TransferBetweenLevelsTypes |
NcmPlanarBuilder.TransferBetweenLevelsTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NcmPlanarBuilder.TransferBetweenLevelsTypes |
NcmPlanarBuilder.TransferBetweenLevelsTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NcmPlanarBuilder.TransferBetweenLevelsTypes[] |
NcmPlanarBuilder.TransferBetweenLevelsTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NcmPlanarBuilder.setTransferBetweenLevelsType(NcmPlanarBuilder.TransferBetweenLevelsTypes transferType)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.