Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static NcmEngRetBuilder.EngageRetractTypes |
NcmEngRetBuilder.EngageRetractTypes.LINEAR
Linear
|
static NcmEngRetBuilder.EngageRetractTypes |
NcmEngRetBuilder.EngageRetractTypes.NONE
None
|
static NcmEngRetBuilder.EngageRetractTypes |
NcmEngRetBuilder.EngageRetractTypes.PLUNGE_LIFT
Plunge Engage/Lift Retract
|
static NcmEngRetBuilder.EngageRetractTypes |
NcmEngRetBuilder.EngageRetractTypes.SMOOTH
Smooth connections
|
Modifier and Type | Method and Description |
---|---|
NcmEngRetBuilder.EngageRetractTypes |
NcmEngRetBuilder.engageRetractType()
Returns the type of engage/retract
License requirements: None. |
static NcmEngRetBuilder.EngageRetractTypes |
NcmEngRetBuilder.EngageRetractTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NcmEngRetBuilder.EngageRetractTypes |
NcmEngRetBuilder.EngageRetractTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NcmEngRetBuilder.EngageRetractTypes[] |
NcmEngRetBuilder.EngageRetractTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NcmEngRetBuilder.setEngageRetractType(NcmEngRetBuilder.EngageRetractTypes newValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.