Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static MultiBladeGeomBuilder.PartAxisOfRotationTypes |
MultiBladeGeomBuilder.PartAxisOfRotationTypes.SPECIFY
Specify
|
static MultiBladeGeomBuilder.PartAxisOfRotationTypes |
MultiBladeGeomBuilder.PartAxisOfRotationTypes.ZM
+ZM
|
Modifier and Type | Method and Description |
---|---|
MultiBladeGeomBuilder.PartAxisOfRotationTypes |
MultiBladeGeomBuilder.axisOfRotation()
Returns the axis of rotation mode
License requirements: None. |
static MultiBladeGeomBuilder.PartAxisOfRotationTypes |
MultiBladeGeomBuilder.PartAxisOfRotationTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MultiBladeGeomBuilder.PartAxisOfRotationTypes |
MultiBladeGeomBuilder.PartAxisOfRotationTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MultiBladeGeomBuilder.PartAxisOfRotationTypes[] |
MultiBladeGeomBuilder.PartAxisOfRotationTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MultiBladeGeomBuilder.setAxisOfRotation(MultiBladeGeomBuilder.PartAxisOfRotationTypes axis)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.