Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static MillOperationBuilder.WallCleanupTypes |
MillOperationBuilder.WallCleanupTypes.AT_END
wall cleanup: at end
|
static MillOperationBuilder.WallCleanupTypes |
MillOperationBuilder.WallCleanupTypes.AT_START
wall cleanup: at start
|
static MillOperationBuilder.WallCleanupTypes |
MillOperationBuilder.WallCleanupTypes.AUTOMATIC
wall cleanup: automatic; not valid for surface contour - boundary drive method
|
static MillOperationBuilder.WallCleanupTypes |
MillOperationBuilder.WallCleanupTypes.NONE
wall cleanup: none
|
Modifier and Type | Method and Description |
---|---|
static MillOperationBuilder.WallCleanupTypes |
MillOperationBuilder.WallCleanupTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MillOperationBuilder.WallCleanupTypes |
MillOperationBuilder.WallCleanupTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MillOperationBuilder.WallCleanupTypes[] |
MillOperationBuilder.WallCleanupTypes.values()
Returns an array that contains the values for this enum.
|
MillOperationBuilder.WallCleanupTypes |
MillOperationBuilder.wallCleanupType()
Returns the wall cleanup mode
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
MillOperationBuilder.setWallCleanupType(MillOperationBuilder.WallCleanupTypes mode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.