Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Method and Description |
---|---|
ManualFeatureBuilder |
FeatureRecognitionBuilder.createManualFeatureBuilder()
Creates a new manual feature builder
License requirements: None. |
ManualFeatureBuilder |
ManualFeatureBuilderList.findItem(int index)
Returns the object at the input index.
|
ManualFeatureBuilder[] |
ManualFeatureBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ManualFeatureBuilderList.append(ManualFeatureBuilder object)
Appends an object to the list
License requirements: None. |
void |
ManualFeatureBuilderList.append(ManualFeatureBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ManualFeatureBuilderList.erase(ManualFeatureBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
ManualFeatureBuilderList.erase(ManualFeatureBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ManualFeatureBuilderList.findIndex(ManualFeatureBuilder obj)
Finds the index where the input object appears.
|
void |
ManualFeatureBuilderList.insert(int location,
ManualFeatureBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
ManualFeatureBuilderList.setContents(ManualFeatureBuilder[] objects)
Sets the contents of the entire list.
|
void |
ManualFeatureBuilderList.swap(ManualFeatureBuilder object1,
ManualFeatureBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.