Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static LaserControlPoint.HeadOrientTypes |
LaserControlPoint.HeadOrientTypes.DYNAMIC
Dynamic
|
static LaserControlPoint.HeadOrientTypes |
LaserControlPoint.HeadOrientTypes.NONE
None
|
static LaserControlPoint.HeadOrientTypes |
LaserControlPoint.HeadOrientTypes.SPECIFY
Specify
|
Modifier and Type | Method and Description |
---|---|
LaserControlPoint.HeadOrientTypes |
LaserControlPoint.localHeadOrientType()
Returns the Local Head Orientation Type
License requirements: None. |
static LaserControlPoint.HeadOrientTypes |
LaserControlPoint.HeadOrientTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LaserControlPoint.HeadOrientTypes |
LaserControlPoint.HeadOrientTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LaserControlPoint.HeadOrientTypes[] |
LaserControlPoint.HeadOrientTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LaserControlPoint.setLocalHeadOrientType(LaserControlPoint.HeadOrientTypes type)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.