Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static InspectionUVGridBuilder.SphereAxisType |
InspectionUVGridBuilder.SphereAxisType.ALIGN_WITH_PROBE
Align with probe axis
|
static InspectionUVGridBuilder.SphereAxisType |
InspectionUVGridBuilder.SphereAxisType.SELECT_DIRECTION
User specified direction
|
static InspectionUVGridBuilder.SphereAxisType |
InspectionUVGridBuilder.SphereAxisType.SETUP_ZAXIS
Z-axis stored in Setup
|
Modifier and Type | Method and Description |
---|---|
InspectionUVGridBuilder.SphereAxisType |
InspectionUVGridBuilder.sphereAxisMethod()
Returns the method for determining the axis for a sphere
License requirements: None. |
static InspectionUVGridBuilder.SphereAxisType |
InspectionUVGridBuilder.SphereAxisType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionUVGridBuilder.SphereAxisType |
InspectionUVGridBuilder.SphereAxisType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionUVGridBuilder.SphereAxisType[] |
InspectionUVGridBuilder.SphereAxisType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InspectionUVGridBuilder.setSphereAxisMethod(InspectionUVGridBuilder.SphereAxisType method)
License requirements: insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.