Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static InspectionToleranceOperationBuilder.ParamExtent |
InspectionToleranceOperationBuilder.ParamExtent.TOTAL
Total
|
static InspectionToleranceOperationBuilder.ParamExtent |
InspectionToleranceOperationBuilder.ParamExtent.UNIT_AREA_LENGTH
Unit Area Length
|
Modifier and Type | Method and Description |
---|---|
InspectionToleranceOperationBuilder.ParamExtent |
InspectionToleranceOperationBuilder.enumParameterExtent()
Returns the enum parameter extent
License requirements: None. |
static InspectionToleranceOperationBuilder.ParamExtent |
InspectionToleranceOperationBuilder.ParamExtent.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionToleranceOperationBuilder.ParamExtent |
InspectionToleranceOperationBuilder.ParamExtent.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionToleranceOperationBuilder.ParamExtent[] |
InspectionToleranceOperationBuilder.ParamExtent.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InspectionToleranceOperationBuilder.setEnumParameterExtent(InspectionToleranceOperationBuilder.ParamExtent enumParameterExtent)
License requirements: insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.