Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static InspectionToleranceOperationBuilder.AngleFormat |
InspectionToleranceOperationBuilder.AngleFormat.DECIMAL_DEGREE
Decimal Degrees
|
static InspectionToleranceOperationBuilder.AngleFormat |
InspectionToleranceOperationBuilder.AngleFormat.DEG_MIN_SEC
Degrees/Minutes/Seconds
|
Modifier and Type | Method and Description |
---|---|
InspectionToleranceOperationBuilder.AngleFormat |
InspectionToleranceOperationBuilder.useDegMin()
Returns the deg/min flag for angle between
License requirements: None. |
static InspectionToleranceOperationBuilder.AngleFormat |
InspectionToleranceOperationBuilder.AngleFormat.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionToleranceOperationBuilder.AngleFormat |
InspectionToleranceOperationBuilder.AngleFormat.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionToleranceOperationBuilder.AngleFormat[] |
InspectionToleranceOperationBuilder.AngleFormat.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InspectionToleranceOperationBuilder.setUseDegMin(InspectionToleranceOperationBuilder.AngleFormat useDegMinSec)
License requirements: insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.