Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static InspectionSurfaceFeatureBuilder.PointDataDefinitionType |
InspectionSurfaceFeatureBuilder.PointDataDefinitionType.INDIVIDUAL_POINTS
Individual points are defined
|
static InspectionSurfaceFeatureBuilder.PointDataDefinitionType |
InspectionSurfaceFeatureBuilder.PointDataDefinitionType.NONE
No point data is defined
|
static InspectionSurfaceFeatureBuilder.PointDataDefinitionType |
InspectionSurfaceFeatureBuilder.PointDataDefinitionType.POINT_SET
A set of points are defined using parameters
|
Modifier and Type | Method and Description |
---|---|
InspectionSurfaceFeatureBuilder.PointDataDefinitionType |
InspectionSurfaceFeatureBuilder.pointDataDefinition()
Returns the point data definition type
License requirements: None. |
static InspectionSurfaceFeatureBuilder.PointDataDefinitionType |
InspectionSurfaceFeatureBuilder.PointDataDefinitionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionSurfaceFeatureBuilder.PointDataDefinitionType |
InspectionSurfaceFeatureBuilder.PointDataDefinitionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionSurfaceFeatureBuilder.PointDataDefinitionType[] |
InspectionSurfaceFeatureBuilder.PointDataDefinitionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InspectionSurfaceFeatureBuilder.setPointDataDefinition(InspectionSurfaceFeatureBuilder.PointDataDefinitionType pointDataDefinition)
License requirements: insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.