Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static InspectionOperationTransformBuilder.Line |
InspectionOperationTransformBuilder.Line.POINT_AND_VECTOR
specify a line by a point and a vector
|
static InspectionOperationTransformBuilder.Line |
InspectionOperationTransformBuilder.Line.SPECIFY
specify a line
|
static InspectionOperationTransformBuilder.Line |
InspectionOperationTransformBuilder.Line.TWO_POINT
specify a line by two point
|
Modifier and Type | Method and Description |
---|---|
InspectionOperationTransformBuilder.Line |
InspectionOperationTransformBuilder.lineMethod()
Returns the line method
License requirements: None. |
static InspectionOperationTransformBuilder.Line |
InspectionOperationTransformBuilder.Line.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionOperationTransformBuilder.Line |
InspectionOperationTransformBuilder.Line.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionOperationTransformBuilder.Line[] |
InspectionOperationTransformBuilder.Line.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InspectionOperationTransformBuilder.setLineMethod(InspectionOperationTransformBuilder.Line lineMethod)
License requirements: insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.