Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static InspectionMethodBuilder.PolarSequenceStartTypes |
InspectionMethodBuilder.PolarSequenceStartTypes.RMAX_AMAX
max Radius - max Angle
|
static InspectionMethodBuilder.PolarSequenceStartTypes |
InspectionMethodBuilder.PolarSequenceStartTypes.RMAX_AMIN
max Radius - min Angle
|
static InspectionMethodBuilder.PolarSequenceStartTypes |
InspectionMethodBuilder.PolarSequenceStartTypes.RMIN_AMAX
min Radius - max Angle
|
static InspectionMethodBuilder.PolarSequenceStartTypes |
InspectionMethodBuilder.PolarSequenceStartTypes.RMIN_AMIN
min Radius - min Angle
|
Modifier and Type | Method and Description |
---|---|
InspectionMethodBuilder.PolarSequenceStartTypes |
InspectionMethodBuilder.polarSequenceStart()
Returns the polar sequence start location
License requirements: None. |
InspectionMethodBuilder.PolarSequenceStartTypes |
InspectionPolarGridBuilder.sequenceStart()
Returns the point sequence start location
License requirements: None. |
static InspectionMethodBuilder.PolarSequenceStartTypes |
InspectionMethodBuilder.PolarSequenceStartTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionMethodBuilder.PolarSequenceStartTypes |
InspectionMethodBuilder.PolarSequenceStartTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionMethodBuilder.PolarSequenceStartTypes[] |
InspectionMethodBuilder.PolarSequenceStartTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InspectionMethodBuilder.setPolarSequenceStart(InspectionMethodBuilder.PolarSequenceStartTypes polSeqStart)
License requirements: insp_programming ("INSPECTION PROGRAMMING") . |
void |
InspectionPolarGridBuilder.setSequenceStart(InspectionMethodBuilder.PolarSequenceStartTypes ptSeqStart)
License requirements: insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.