Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static HoleDrillingBuilder.ControlPointOffsetType |
HoleDrillingBuilder.ControlPointOffsetType.FEATURE
machining feature Z position
|
static HoleDrillingBuilder.ControlPointOffsetType |
HoleDrillingBuilder.ControlPointOffsetType.NONE
in process feature Z position
|
Modifier and Type | Method and Description |
---|---|
HoleDrillingBuilder.ControlPointOffsetType |
HoleDrillingBuilder.controlPointOffset()
Returns the control point offset type
License requirements: None. |
static HoleDrillingBuilder.ControlPointOffsetType |
HoleDrillingBuilder.ControlPointOffsetType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HoleDrillingBuilder.ControlPointOffsetType |
HoleDrillingBuilder.ControlPointOffsetType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HoleDrillingBuilder.ControlPointOffsetType[] |
HoleDrillingBuilder.ControlPointOffsetType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HoleDrillingBuilder.setControlPointOffset(HoleDrillingBuilder.ControlPointOffsetType currentValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.