Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Interface and Description |
---|---|
interface |
ThreadedBossSet
Represents a thread boss Geometry builder
To create a new instance of this class, use HoleBossGeom.createThreadedBossBuilder(nxopen.NXObject[], double, double, nxopen.NXObject, double, double, double, java.lang.String, double, int, nxopen.cam.HoleBossGeom.FormTypes, java.lang.String) Created in NX7.5.0 |
interface |
ThreadedHoleSet
Represents a Cut Area Geometry builder
To create a new instance of this class, use HoleBossGeom.createThreadedHoleBuilder(nxopen.NXObject[], double, double, nxopen.NXObject, double, double, double, java.lang.String, java.lang.String, double, int, nxopen.cam.HoleBossGeom.FormTypes, java.lang.String, java.lang.String, int) Created in NX7.5.0 |
Modifier and Type | Method and Description |
---|---|
HoleBossSet |
HoleBossGeom.createHoleBossBuilder(NXObject[] entities,
double diameter,
double depth,
NXObject toolAxis,
int depthLimit)
Create a new Hole or Boss
License requirements: cam_base ("CAM BASE") . |
HoleBossSet |
HoleBossSetList.findItem(int index)
Returns the object at the input index.
|
HoleBossSet[] |
HoleBossSetList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
HoleBossSetList.append(HoleBossSet object)
Appends an object to the list
License requirements: None. |
void |
HoleBossSetList.append(HoleBossSet[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
HoleBossSetList.erase(HoleBossSet obj)
Erases the object from the list, but does not delete the object.
|
void |
HoleBossSetList.erase(HoleBossSet obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
HoleBossSetList.findIndex(HoleBossSet obj)
Finds the index where the input object appears.
|
void |
HoleBossSetList.insert(int location,
HoleBossSet object)
Inserts an object at the specified location
License requirements: None. |
void |
HoleBossSetList.setContents(HoleBossSet[] objects)
Sets the contents of the entire list.
|
void |
HoleBossSetList.swap(HoleBossSet object1,
HoleBossSet object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.