Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static HoleBossGeom.DepthLimitTypes |
HoleBossGeom.DepthLimitTypes.BLIND
Deprecated.
Depth Limit: Blind
|
static HoleBossGeom.DepthLimitTypes |
HoleBossGeom.DepthLimitTypes.THROUGH
Deprecated.
Depth Limit: Through
|
static HoleBossGeom.DepthLimitTypes |
HoleBossGeom.DepthLimitTypes.UNKNOWN
Deprecated.
It maybe mixed type with both Through and Blind features in NX8.
|
Modifier and Type | Method and Description |
---|---|
HoleBossGeom.DepthLimitTypes |
HoleBossGeom.depthLimit()
Deprecated.
Deprecated in NX8.0.0. Use
HoleBossSet.depthLimit() instead.
|
static HoleBossGeom.DepthLimitTypes |
HoleBossGeom.DepthLimitTypes.valueOf(int value)
Deprecated.
Returns the enum constant of the specified enum type with the specified value.
|
static HoleBossGeom.DepthLimitTypes |
HoleBossGeom.DepthLimitTypes.valueOf(String name)
Deprecated.
Returns the enum constant of the specified enum type with the specified name.
|
static HoleBossGeom.DepthLimitTypes[] |
HoleBossGeom.DepthLimitTypes.values()
Deprecated.
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HoleBossGeom.setDepthLimit(HoleBossGeom.DepthLimitTypes type)
Deprecated.
Deprecated in NX8.0.0. Use
HoleBossSet.setDepthLimit(nxopen.cam.HoleBossSet.DepthLimitTypes) instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.