Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static GuidedCurveCutOrder.CutOrderOption |
GuidedCurveCutOrder.CutOrderOption.AWAY |
static GuidedCurveCutOrder.CutOrderOption |
GuidedCurveCutOrder.CutOrderOption.FROM_FIRST_CURVE |
static GuidedCurveCutOrder.CutOrderOption |
GuidedCurveCutOrder.CutOrderOption.INSIDE_OUT_ALTERNATE |
static GuidedCurveCutOrder.CutOrderOption |
GuidedCurveCutOrder.CutOrderOption.LEFT_TO_RIGHT |
static GuidedCurveCutOrder.CutOrderOption |
GuidedCurveCutOrder.CutOrderOption.OUTSIDE_IN_ALTERNATE |
static GuidedCurveCutOrder.CutOrderOption |
GuidedCurveCutOrder.CutOrderOption.RIGHT_TO_LEFT |
static GuidedCurveCutOrder.CutOrderOption |
GuidedCurveCutOrder.CutOrderOption.TOWARD |
Modifier and Type | Method and Description |
---|---|
GuidedCurveCutOrder.CutOrderOption |
GuidedCurveCutOrder.cutOrderType()
Returns the cut order
License requirements: None. |
static GuidedCurveCutOrder.CutOrderOption |
GuidedCurveCutOrder.CutOrderOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GuidedCurveCutOrder.CutOrderOption |
GuidedCurveCutOrder.CutOrderOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GuidedCurveCutOrder.CutOrderOption[] |
GuidedCurveCutOrder.CutOrderOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GuidedCurveCutOrder.setCutOrderType(GuidedCurveCutOrder.CutOrderOption cutOrder)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.