Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static GroupFeatures.FeaturesToGroupTypes |
GroupFeatures.FeaturesToGroupTypes.ALL |
static GroupFeatures.FeaturesToGroupTypes |
GroupFeatures.FeaturesToGroupTypes.BELOW_TOP_FACE |
static GroupFeatures.FeaturesToGroupTypes |
GroupFeatures.FeaturesToGroupTypes.SPECIFY_FEATURES |
Modifier and Type | Method and Description |
---|---|
GroupFeatures.FeaturesToGroupTypes |
GroupFeatures.featuresToGroupType()
Returns the features to group enumeration
License requirements: None. |
static GroupFeatures.FeaturesToGroupTypes |
GroupFeatures.FeaturesToGroupTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GroupFeatures.FeaturesToGroupTypes |
GroupFeatures.FeaturesToGroupTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GroupFeatures.FeaturesToGroupTypes[] |
GroupFeatures.FeaturesToGroupTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GroupFeatures.setFeaturesToGroupType(GroupFeatures.FeaturesToGroupTypes groupType)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.