Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static GrooveToolBuilder.HolderStyles |
GrooveToolBuilder.HolderStyles.DEG0
0 degrees
|
static GrooveToolBuilder.HolderStyles |
GrooveToolBuilder.HolderStyles.DEG45
45 degrees
|
static GrooveToolBuilder.HolderStyles |
GrooveToolBuilder.HolderStyles.DEG90
90 degrees
|
static GrooveToolBuilder.HolderStyles |
GrooveToolBuilder.HolderStyles.USER_DEFINED
user defined
|
Modifier and Type | Method and Description |
---|---|
GrooveToolBuilder.HolderStyles |
GrooveToolBuilder.holderStyle()
Returns the holder style
License requirements: None. |
static GrooveToolBuilder.HolderStyles |
GrooveToolBuilder.HolderStyles.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GrooveToolBuilder.HolderStyles |
GrooveToolBuilder.HolderStyles.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GrooveToolBuilder.HolderStyles[] |
GrooveToolBuilder.HolderStyles.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GrooveToolBuilder.setHolderStyle(GrooveToolBuilder.HolderStyles holderStyle)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.