Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static GougeCheckBuilder.GougeCheckStock |
GougeCheckBuilder.GougeCheckStock.AUTOMATIC
use automatic
|
static GougeCheckBuilder.GougeCheckStock |
GougeCheckBuilder.GougeCheckStock.USER_DEFINED
use user defined
|
Modifier and Type | Method and Description |
---|---|
GougeCheckBuilder.GougeCheckStock |
GougeCheckBuilder.gougeCheckStockOptions()
Returns the gouge check stock options.
|
static GougeCheckBuilder.GougeCheckStock |
GougeCheckBuilder.GougeCheckStock.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GougeCheckBuilder.GougeCheckStock |
GougeCheckBuilder.GougeCheckStock.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GougeCheckBuilder.GougeCheckStock[] |
GougeCheckBuilder.GougeCheckStock.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GougeCheckBuilder.setGougeCheckStockOptions(GougeCheckBuilder.GougeCheckStock options)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.