Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static GeometryGroup.DirectionTypes |
GeometryGroup.DirectionTypes.SPECIFY
derived blank direction using user defined
|
static GeometryGroup.DirectionTypes |
GeometryGroup.DirectionTypes.ZM
derived blank direction using ZM
|
Modifier and Type | Method and Description |
---|---|
GeometryGroup.DirectionTypes |
GeometryGroup.directionType()
Returns the derived blank orientation type
License requirements: None. |
static GeometryGroup.DirectionTypes |
GeometryGroup.DirectionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeometryGroup.DirectionTypes |
GeometryGroup.DirectionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeometryGroup.DirectionTypes[] |
GeometryGroup.DirectionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GeometryGroup.setDirectionType(GeometryGroup.DirectionTypes newValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.