Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static FollowPartMoveBuilder.MoveDirectionTypes |
FollowPartMoveBuilder.MoveDirectionTypes.FORWARD |
static FollowPartMoveBuilder.MoveDirectionTypes |
FollowPartMoveBuilder.MoveDirectionTypes.REVERSE |
static FollowPartMoveBuilder.MoveDirectionTypes |
FollowPartMoveBuilder.MoveDirectionTypes.UNDEFINED |
Modifier and Type | Method and Description |
---|---|
FollowPartMoveBuilder.MoveDirectionTypes |
FollowPartMoveBuilder.moveDirection()
Returns the move direction
License requirements: None. |
static FollowPartMoveBuilder.MoveDirectionTypes |
FollowPartMoveBuilder.MoveDirectionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FollowPartMoveBuilder.MoveDirectionTypes |
FollowPartMoveBuilder.MoveDirectionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FollowPartMoveBuilder.MoveDirectionTypes[] |
FollowPartMoveBuilder.MoveDirectionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FollowPartMoveBuilder.setMoveDirection(FollowPartMoveBuilder.MoveDirectionTypes direction)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.