Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static FirstPlunge.Positions |
FirstPlunge.Positions.AUTOMATIC
Automatic
|
static FirstPlunge.Positions |
FirstPlunge.Positions.AXIAL_OR_RADIAL
Axial Radial
|
static FirstPlunge.Positions |
FirstPlunge.Positions.SPECIFIED
Specify
|
Modifier and Type | Method and Description |
---|---|
FirstPlunge.Positions |
FirstPlunge.position()
Returns the first plunge position
License requirements: None. |
static FirstPlunge.Positions |
FirstPlunge.Positions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FirstPlunge.Positions |
FirstPlunge.Positions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FirstPlunge.Positions[] |
FirstPlunge.Positions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FirstPlunge.setPosition(FirstPlunge.Positions position)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.