Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static DmRotaryFloorFinishBuilder.DirectionType |
DmRotaryFloorFinishBuilder.DirectionType.ALONG_AXIS
along axis
|
static DmRotaryFloorFinishBuilder.DirectionType |
DmRotaryFloorFinishBuilder.DirectionType.AROUND_AXIS
around axis
|
Modifier and Type | Method and Description |
---|---|
DmRotaryFloorFinishBuilder.DirectionType |
DmRotaryFloorFinishBuilder.directionAxisType()
Returns the direction axis type
License requirements: None. |
static DmRotaryFloorFinishBuilder.DirectionType |
DmRotaryFloorFinishBuilder.DirectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DmRotaryFloorFinishBuilder.DirectionType |
DmRotaryFloorFinishBuilder.DirectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DmRotaryFloorFinishBuilder.DirectionType[] |
DmRotaryFloorFinishBuilder.DirectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DmRotaryFloorFinishBuilder.setDirectionAxisType(DmRotaryFloorFinishBuilder.DirectionType directionType)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.