Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static DmCmBuilder.ExtDisType |
DmCmBuilder.ExtDisType.FIXED
Specify
|
static DmCmBuilder.ExtDisType |
DmCmBuilder.ExtDisType.NONE
None
|
static DmCmBuilder.ExtDisType |
DmCmBuilder.ExtDisType.PERCENT
Tool Diameter
|
Modifier and Type | Method and Description |
---|---|
DmCmBuilder.ExtDisType |
DmCmBuilder.dmCmEndCutDisType()
Deprecated.
Deprecated in NX8.5.0. Use
DmCmBuilder.endExtDistSpecValueBuilder() instead.
|
DmCmBuilder.ExtDisType |
DmCmBuilder.dmCmStartCutDisType()
Deprecated.
Deprecated in NX8.5.0. Use
DmCmBuilder.startExtDistSpecValueBuilder() instead.
|
static DmCmBuilder.ExtDisType |
DmCmBuilder.ExtDisType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DmCmBuilder.ExtDisType |
DmCmBuilder.ExtDisType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DmCmBuilder.ExtDisType[] |
DmCmBuilder.ExtDisType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DmCmBuilder.setDmCmEndCutDisType(DmCmBuilder.ExtDisType dmCmEndCutDisType)
Deprecated.
Deprecated in NX8.5.0. Use
DmCmBuilder.endExtDistSpecValueBuilder() instead.
|
void |
DmCmBuilder.setDmCmStartCutDisType(DmCmBuilder.ExtDisType dmCmStartCutDisType)
Deprecated.
Deprecated in NX8.5.0. Use
DmCmBuilder.startExtDistSpecValueBuilder() instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.