Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static DmBndBuilder.BndPatternCenterTypes |
DmBndBuilder.BndPatternCenterTypes.METHOD_AUTOMATIC
Automatic
|
static DmBndBuilder.BndPatternCenterTypes |
DmBndBuilder.BndPatternCenterTypes.METHOD_SPECIFY
Specify
|
Modifier and Type | Method and Description |
---|---|
DmBndBuilder.BndPatternCenterTypes |
DmBndBuilder.cutPatternCenter()
Returns the Pattern Center
License requirements: None. |
static DmBndBuilder.BndPatternCenterTypes |
DmBndBuilder.BndPatternCenterTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DmBndBuilder.BndPatternCenterTypes |
DmBndBuilder.BndPatternCenterTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DmBndBuilder.BndPatternCenterTypes[] |
DmBndBuilder.BndPatternCenterTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DmBndBuilder.setCutPatternCenter(DmBndBuilder.BndPatternCenterTypes patternCenterValue)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.