Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static DmBndBuilder.BndCustomStartTypes |
DmBndBuilder.BndCustomStartTypes.AUTOMATIC
Boundary Milling Custom Start Automatic
|
static DmBndBuilder.BndCustomStartTypes |
DmBndBuilder.BndCustomStartTypes.CUSTOM
Boundary Milling Custom Start Custom
|
Modifier and Type | Method and Description |
---|---|
DmBndBuilder.BndCustomStartTypes |
DmBndBuilder.bndCustomStart()
Returns the Custom Start
License requirements: None. |
static DmBndBuilder.BndCustomStartTypes |
DmBndBuilder.BndCustomStartTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DmBndBuilder.BndCustomStartTypes |
DmBndBuilder.BndCustomStartTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DmBndBuilder.BndCustomStartTypes[] |
DmBndBuilder.BndCustomStartTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DmBndBuilder.setBndCustomStart(DmBndBuilder.BndCustomStartTypes customStartValue)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.