Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static DmAmBuilder.SteepOverlapOptTypes |
DmAmBuilder.SteepOverlapOptTypes.ANGLE
Angle Overlap
|
static DmAmBuilder.SteepOverlapOptTypes |
DmAmBuilder.SteepOverlapOptTypes.DISTANCE
Distance Overlap
|
static DmAmBuilder.SteepOverlapOptTypes |
DmAmBuilder.SteepOverlapOptTypes.NONE
No Overlap
|
Modifier and Type | Method and Description |
---|---|
DmAmBuilder.SteepOverlapOptTypes |
DmAmBuilder.steepOverlapType()
Returns the Steep Overlap Type
License requirements: None. |
static DmAmBuilder.SteepOverlapOptTypes |
DmAmBuilder.SteepOverlapOptTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DmAmBuilder.SteepOverlapOptTypes |
DmAmBuilder.SteepOverlapOptTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DmAmBuilder.SteepOverlapOptTypes[] |
DmAmBuilder.SteepOverlapOptTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DmAmBuilder.setSteepOverlapType(DmAmBuilder.SteepOverlapOptTypes steepOverlapType)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.