Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static DmAmBuilder.AmCustomStartTypes |
DmAmBuilder.AmCustomStartTypes.AUTOMATIC
Area Milling Custom Start Automatic
|
static DmAmBuilder.AmCustomStartTypes |
DmAmBuilder.AmCustomStartTypes.CUSTOM
Area Milling Custom Start Custom
|
Modifier and Type | Method and Description |
---|---|
DmAmBuilder.AmCustomStartTypes |
DmAmBuilder.amCutRegionStartEnum()
Returns the Cut Region Start Point
License requirements: None. |
static DmAmBuilder.AmCustomStartTypes |
DmAmBuilder.AmCustomStartTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DmAmBuilder.AmCustomStartTypes |
DmAmBuilder.AmCustomStartTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DmAmBuilder.AmCustomStartTypes[] |
DmAmBuilder.AmCustomStartTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DmAmBuilder.setAmCutRegionStartEnum(DmAmBuilder.AmCustomStartTypes amCutRegionStart)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.