Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static DPMItpBuilder.StepMethodOption |
DPMItpBuilder.StepMethodOption.POINTS |
static DPMItpBuilder.StepMethodOption |
DPMItpBuilder.StepMethodOption.TOLERANCE |
Modifier and Type | Method and Description |
---|---|
DPMItpBuilder.StepMethodOption |
DmStreamlineCutStep.cutStepType()
Returns the cut step type which defines different cut steps including tolerances and points number
License requirements: None. |
DPMItpBuilder.StepMethodOption |
DPMItpBuilder.stepMethod()
Deprecated.
Deprecated in NX10.0.1. Use
DmStreamlineCutStep.cutStepType() and DmStreamlineCutStep.setCutStepType(nxopen.cam.DPMItpBuilder.StepMethodOption) instead.
|
static DPMItpBuilder.StepMethodOption |
DPMItpBuilder.StepMethodOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DPMItpBuilder.StepMethodOption |
DPMItpBuilder.StepMethodOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DPMItpBuilder.StepMethodOption[] |
DPMItpBuilder.StepMethodOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DmStreamlineCutStep.setCutStepType(DPMItpBuilder.StepMethodOption type)
License requirements: cam_base ("CAM BASE") . |
void |
DPMItpBuilder.setStepMethod(DPMItpBuilder.StepMethodOption stepMethod)
Deprecated.
Deprecated in NX10.0.1. Use
DmStreamlineCutStep.cutStepType() and DmStreamlineCutStep.setCutStepType(nxopen.cam.DPMItpBuilder.StepMethodOption) instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.