Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static DPMItpBuilder.SelectionMethodOption |
DPMItpBuilder.SelectionMethodOption.AUTOMATIC
automatic
|
static DPMItpBuilder.SelectionMethodOption |
DPMItpBuilder.SelectionMethodOption.ON_PART
on part
|
static DPMItpBuilder.SelectionMethodOption |
DPMItpBuilder.SelectionMethodOption.SPECIFY
specify
|
Modifier and Type | Method and Description |
---|---|
DPMItpBuilder.SelectionMethodOption |
DPMItpBuilder.selectionMethod()
Returns the flow and cross selection method
License requirements: cam_base ("CAM BASE") . |
static DPMItpBuilder.SelectionMethodOption |
DPMItpBuilder.SelectionMethodOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DPMItpBuilder.SelectionMethodOption |
DPMItpBuilder.SelectionMethodOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DPMItpBuilder.SelectionMethodOption[] |
DPMItpBuilder.SelectionMethodOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DPMItpBuilder.setSelectionMethod(DPMItpBuilder.SelectionMethodOption selectionMethod)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.