Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static DPMItpBuilder.CrossCurvesMethodOption |
DPMItpBuilder.CrossCurvesMethodOption.NORMAL_TO_FLOW
normal to flow
|
static DPMItpBuilder.CrossCurvesMethodOption |
DPMItpBuilder.CrossCurvesMethodOption.ON_PART
on part
|
Modifier and Type | Method and Description |
---|---|
DPMItpBuilder.CrossCurvesMethodOption |
DPMItpBuilder.crossCurvesMethod()
Returns the cross curves selection method
License requirements: cam_base ("CAM BASE") . |
static DPMItpBuilder.CrossCurvesMethodOption |
DPMItpBuilder.CrossCurvesMethodOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DPMItpBuilder.CrossCurvesMethodOption |
DPMItpBuilder.CrossCurvesMethodOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DPMItpBuilder.CrossCurvesMethodOption[] |
DPMItpBuilder.CrossCurvesMethodOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DPMItpBuilder.setCrossCurvesMethod(DPMItpBuilder.CrossCurvesMethodOption crossCurvesMethod)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.