Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static CylinderMillingBuilder.BlankDiameterTypes |
CylinderMillingBuilder.BlankDiameterTypes.DIAMETER
Diameter
|
static CylinderMillingBuilder.BlankDiameterTypes |
CylinderMillingBuilder.BlankDiameterTypes.DISTANCE
distance
|
Modifier and Type | Method and Description |
---|---|
CylinderMillingBuilder.BlankDiameterTypes |
CylinderMillingBuilder.blankDiameter()
Returns the start location
License requirements: None. |
static CylinderMillingBuilder.BlankDiameterTypes |
CylinderMillingBuilder.BlankDiameterTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CylinderMillingBuilder.BlankDiameterTypes |
CylinderMillingBuilder.BlankDiameterTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CylinderMillingBuilder.BlankDiameterTypes[] |
CylinderMillingBuilder.BlankDiameterTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CylinderMillingBuilder.setBlankDiameter(CylinderMillingBuilder.BlankDiameterTypes newValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.