Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static CutParametersTrimControlTypes |
CutParametersTrimControlTypes.EXTERIOR_EDGES
exterior edges
|
static CutParametersTrimControlTypes |
CutParametersTrimControlTypes.NONE
none
|
static CutParametersTrimControlTypes |
CutParametersTrimControlTypes.SILHOUTTE
silhoutte type
|
Modifier and Type | Method and Description |
---|---|
CutParametersTrimControlTypes |
MillCutParameters.trimControl()
Returns the trim control method type
License requirements: None. |
static CutParametersTrimControlTypes |
CutParametersTrimControlTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CutParametersTrimControlTypes |
CutParametersTrimControlTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CutParametersTrimControlTypes[] |
CutParametersTrimControlTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MillCutParameters.setTrimControl(CutParametersTrimControlTypes propValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.