Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Method and Description |
---|---|
CustomLoopSet |
CustomLoops.createLoopSet()
Deprecated.
Deprecated in NX9.0.0. Use
PatchOpeningsBuilder instead.
|
CustomLoopSet |
CustomLoopSetList.findItem(int index)
Returns the object at the input index.
|
CustomLoopSet[] |
CustomLoopSetList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
CustomLoopSetList.append(CustomLoopSet object)
Appends an object to the list
License requirements: None. |
void |
CustomLoopSetList.append(CustomLoopSet[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
CustomLoopSetList.erase(CustomLoopSet obj)
Erases the object from the list, but does not delete the object.
|
void |
CustomLoopSetList.erase(CustomLoopSet obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
CustomLoopSetList.findIndex(CustomLoopSet obj)
Finds the index where the input object appears.
|
void |
CustomLoopSetList.insert(int location,
CustomLoopSet object)
Inserts an object at the specified location
License requirements: None. |
void |
CustomLoopSetList.setContents(CustomLoopSet[] objects)
Sets the contents of the entire list.
|
void |
CustomLoopSetList.swap(CustomLoopSet object1,
CustomLoopSet object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.