Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static ConvertFromMCDBuilder.PocketLocationTypes |
ConvertFromMCDBuilder.PocketLocationTypes.SPINDLE |
static ConvertFromMCDBuilder.PocketLocationTypes |
ConvertFromMCDBuilder.PocketLocationTypes.TOOL_MAGAZINE |
Modifier and Type | Method and Description |
---|---|
ConvertFromMCDBuilder.PocketLocationTypes |
ConvertFromMCDBuilder.millPocketLocation()
Returns the mill pocket location
License requirements: None. |
static ConvertFromMCDBuilder.PocketLocationTypes |
ConvertFromMCDBuilder.PocketLocationTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ConvertFromMCDBuilder.PocketLocationTypes |
ConvertFromMCDBuilder.PocketLocationTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ConvertFromMCDBuilder.PocketLocationTypes[] |
ConvertFromMCDBuilder.PocketLocationTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ConvertFromMCDBuilder.setMillPocketLocation(ConvertFromMCDBuilder.PocketLocationTypes pocketPosition)
License requirements: ug_isv_full ("Full functionality for Integrated Simulation and Verification") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.