Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
nxopen.sim |
Provides classes and interfaces for Machine Tool Builder and CAM-Simulation.
|
Modifier and Type | Method and Description |
---|---|
CollisionPairBuilder |
CollisionPairBuilderList.findItem(int index)
Returns the object at the input index.
|
CollisionPairBuilder[] |
CollisionPairBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
CollisionPairBuilderList.append(CollisionPairBuilder object)
Appends an object to the list
License requirements: None. |
void |
CollisionPairBuilderList.append(CollisionPairBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
CollisionPairBuilderList.erase(CollisionPairBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
CollisionPairBuilderList.erase(CollisionPairBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
CollisionPairBuilderList.findIndex(CollisionPairBuilder obj)
Finds the index where the input object appears.
|
void |
CollisionPairBuilderList.insert(int location,
CollisionPairBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
CollisionPairBuilderList.setContents(CollisionPairBuilder[] objects)
Sets the contents of the entire list.
|
void |
CollisionPairBuilderList.swap(CollisionPairBuilder object1,
CollisionPairBuilder object2)
Exchanges the position of two objects inside the list.
|
Modifier and Type | Method and Description |
---|---|
CollisionPairBuilder |
KinematicConfigurator.createCollisionPairBuilder()
Creates a collision pair builder
License requirements: ug_isv_full ("Full functionality for Integrated Simulation and Verification") OR nx_isv_mtb ("Machine Tool Builder") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.