Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static CenterlineDrillTurningBuilder.StartPositionTypes |
CenterlineDrillTurningBuilder.StartPositionTypes.AUTOMATIC
Start Position: Automatic
|
static CenterlineDrillTurningBuilder.StartPositionTypes |
CenterlineDrillTurningBuilder.StartPositionTypes.SPECIFY
Start Position: Specify
|
Modifier and Type | Method and Description |
---|---|
CenterlineDrillTurningBuilder.StartPositionTypes |
CenterlineDrillTurningBuilder.startPosition()
Returns the start position
License requirements: None. |
static CenterlineDrillTurningBuilder.StartPositionTypes |
CenterlineDrillTurningBuilder.StartPositionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CenterlineDrillTurningBuilder.StartPositionTypes |
CenterlineDrillTurningBuilder.StartPositionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CenterlineDrillTurningBuilder.StartPositionTypes[] |
CenterlineDrillTurningBuilder.StartPositionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CenterlineDrillTurningBuilder.setStartPosition(CenterlineDrillTurningBuilder.StartPositionTypes startPositionMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.