Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static CamPathDir |
CamPathDir.CLOCKWISE |
static CamPathDir |
CamPathDir.COUNTERCLOCKWISE |
Modifier and Type | Method and Description |
---|---|
CamPathDir |
PathContactMotion.arcDirection()
Returns the direction of the arc of the contact motion if the shape is circular
License requirements: None. |
CamPathDir |
PathCircularMotion.direction()
Returns the direction of the arc motion
License requirements: None. |
static CamPathDir |
CamPathDir.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CamPathDir |
CamPathDir.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CamPathDir[] |
CamPathDir.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PathContactMotion.setArcDirection(CamPathDir arcDirection)
License requirements: cam_base ("CAM BASE") . |
void |
PathCircularMotion.setDirection(CamPathDir arcDirection)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.