Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static CamPathContactType |
CamPathContactType.NONE |
static CamPathContactType |
CamPathContactType.THREE_DIMENSIONAL |
static CamPathContactType |
CamPathContactType.TWO_DIMENSIONAL |
Modifier and Type | Method and Description |
---|---|
CamPathContactType |
Path.contactType()
Returns the contact type of the path
License requirements: None. |
static CamPathContactType |
CamPathContactType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CamPathContactType |
CamPathContactType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CamPathContactType[] |
CamPathContactType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Path.setContactType(CamPathContactType contactType)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.