Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static CAMFeature.ProcessStatus |
CAMFeature.ProcessStatus.COMPLETE
The feature's operation toolpaths are complete
|
static CAMFeature.ProcessStatus |
CAMFeature.ProcessStatus.EMPTY
Feature has no operations
|
static CAMFeature.ProcessStatus |
CAMFeature.ProcessStatus.INCOMPLETE
One or more of the feature's operation toolpaths are not completed
|
static CAMFeature.ProcessStatus |
CAMFeature.ProcessStatus.REGENERATE
One or more of the feature's operation toolpaths need to regenerate
|
Modifier and Type | Method and Description |
---|---|
CAMFeature.ProcessStatus |
CAMFeature.getProcessStatus(NCGroup group)
Get the process status of the CAMFeature in the context of a feature group
License requirements: None. |
static CAMFeature.ProcessStatus |
CAMFeature.ProcessStatus.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CAMFeature.ProcessStatus |
CAMFeature.ProcessStatus.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CAMFeature.ProcessStatus[] |
CAMFeature.ProcessStatus.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.