Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Method and Description |
---|---|
BoundaryTurnVariableStockSet |
BoundaryTurnVariableStock.createItemBuilder()
Create a new set
License requirements: cam_base ("CAM BASE") . |
BoundaryTurnVariableStockSet |
BoundaryTurnVariableStockSetList.findItem(int index)
Returns the object at the input index.
|
BoundaryTurnVariableStockSet[] |
BoundaryTurnVariableStockSetList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
BoundaryTurnVariableStockSetList.append(BoundaryTurnVariableStockSet object)
Appends an object to the list
License requirements: None. |
void |
BoundaryTurnVariableStockSetList.append(BoundaryTurnVariableStockSet[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
BoundaryTurnVariableStockSetList.erase(BoundaryTurnVariableStockSet obj)
Erases the object from the list, but does not delete the object.
|
void |
BoundaryTurnVariableStockSetList.erase(BoundaryTurnVariableStockSet obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
BoundaryTurnVariableStockSetList.findIndex(BoundaryTurnVariableStockSet obj)
Finds the index where the input object appears.
|
void |
BoundaryTurnVariableStockSetList.insert(int location,
BoundaryTurnVariableStockSet object)
Inserts an object at the specified location
License requirements: None. |
void |
BoundaryTurnVariableStockSetList.setContents(BoundaryTurnVariableStockSet[] objects)
Sets the contents of the entire list.
|
void |
BoundaryTurnVariableStockSetList.swap(BoundaryTurnVariableStockSet object1,
BoundaryTurnVariableStockSet object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.