Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Interface and Description |
---|---|
interface |
BoundaryMillingSet
Represents a boundary milling set.
|
interface |
BoundarySetPlanarMill
Represents a boundary set for the planar mill/surface contour operation
To create a new instance of this class, use Boundary.createBoundarySetPlanarMill() Created in NX11.0.1 |
interface |
BoundaryTurnSet
Represents a boundary turning set.
|
Modifier and Type | Method and Description |
---|---|
BoundarySet[] |
Boundary.appendFaceBoundary(TaggedObject face,
boolean ignoreHole,
boolean ignoreIsland,
boolean ignoreChamfer,
BoundarySet.ToolSideTypes toolSide)
Append the face boundary
License requirements: cam_base ("CAM BASE") . |
BoundarySet[] |
BoundaryPlanarMill.appendFaceBoundary(TaggedObject face,
boolean ignoreHole,
boolean ignoreIsland,
boolean ignoreChamfer,
BoundarySet.ToolSideTypes toolSide,
int convexEdges,
int concaveEdges)
Append the face boundary
License requirements: cam_base ("CAM BASE") . |
BoundarySet |
Boundary.createBoundarySet()
Create an empty boundary set
License requirements: cam_base ("CAM BASE") . |
BoundarySet |
BoundarySetList.findItem(int index)
Returns the object at the input index.
|
BoundarySet[] |
BoundarySetList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
BoundarySetList.append(BoundarySet object)
Appends an object to the list
License requirements: None. |
void |
BoundarySetList.append(BoundarySet[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
BoundarySetList.erase(BoundarySet obj)
Erases the object from the list, but does not delete the object.
|
void |
BoundarySetList.erase(BoundarySet obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
BoundarySetList.findIndex(BoundarySet obj)
Finds the index where the input object appears.
|
void |
BoundarySetList.insert(int location,
BoundarySet object)
Inserts an object at the specified location
License requirements: None. |
void |
BoundarySetList.setContents(BoundarySet[] objects)
Sets the contents of the entire list.
|
void |
BoundarySetList.swap(BoundarySet object1,
BoundarySet object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.